Program Multiple Target Boards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program Multiple Target Boards

2,115 Views
Designer11
Contributor IV

Hello Everyone,

 

We are in the production phase and would like to know would it be possible to use either the (one) Cyclone Pro, or USB multilink to program multiple target boards.  Or does anyone know of any other products in the market  that offer this capability ?

We are using the HCS08 series.

 

 

 

Thanks,

Labels (1)
0 Kudos
Reply
3 Replies

1,663 Views
Juls
Contributor III

we use cyclone pro

but its 1 unit programmed by cyclone

but you can get more cyclone

as a standalone its pretty easy  you dont need a pc conected to program each unit

only a properly configured cyclone

0 Kudos
Reply

1,663 Views
Designer11
Contributor IV

Yes, i am using the cyclone pro too. I tried to connect two boards in parralel to the cyclone but it didn't  work/program.

0 Kudos
Reply

1,663 Views
bigmac
Specialist III

Hello,

 

You cannot parallel two boards!  It is one board at a time connected to a Cyclone, because the BKGD/MS pin utilises data transfer in both directions.

 

The previous comment made referred to the possibility for the Cyclone to operate stand alone, without the need to always be connected to a computer.  This would simplify the use of multiple Cyclone Pros, but still only with a single board connected to each one at any instant.

 

Regards,

Mac

 

 

 

0 Kudos
Reply