Production Burning of My application on MC9S08AC128 Chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Production Burning of My application on MC9S08AC128 Chip

1,478 Views
sbharsha
Contributor I
Hi,
 
I am bit new to this micro-controller.
 
We have developed the application on MC9S08AC128 Chip, for development purpose i used the Code warrior tool. Now We want to go for thr production of our product where i need to Flash the 10K unts of the Chip for consumr products.
 
Please suggest me the ways i can burn the flash with my application.
 
What are the methods i can use can i use UART/any GPIO.
 
Please suggest me.
 
Warm Regards,
Harsha S
Labels (1)
0 Kudos
Reply
2 Replies

875 Views
Ake
Contributor III
Hi,
You should use eg the USB Multilink or the Cyclone Pro from P&E.
There is ofcourse the DEMOAC board, but it is not designed to burn any MCU outside the board.
 
Put a 8 pin connector on your board, pinout see Figure 15-1 in MC9S08AC16 manual and connect the Flash burner.
It is as simple as that!
 
If you want to burn the Flash by some other port, you must first burn the initial program that will burn the final program. (Don't do it!)
 
Regards,
Ake
0 Kudos
Reply

875 Views
sbharsha
Contributor I
Hi,
 
Thanks it helped me alot.
 
Harsha s
 
0 Kudos
Reply