Problems with jb16.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,819件の閲覧回数
nic
Contributor I

I need help, I can't install the drivers por icp programming. I use Windows xp sp2, is this a problem?.

My hardware is ok, Pta0 = 0v, two resistors (470K) pulldown on D+ and D-. If someone can help, thanks. 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,858件の閲覧回数
nic
Contributor I
Thanks, for your help. I proved all that you tell me but I am not sure about the
conection D+ and D-. bye
Message Edited by nic on 2009-09-21 05:15 PM

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,858件の閲覧回数
pgo
Senior Contributor V

Dear Nic,

 

Your description is a bit vague!

 

 Do you mean

1) that the device is not starting in ICP

  or

2) that you can't install the required drivers when it does?

 

For 1) check

Pull-downs on D+/-  (done)

Check that D+ & D- aren't transposed! It is surprisingly easy to do. 

Crystal osc is OK (using a cro if possible), check crystal, caps & resistor.

100nF (or 470nF advice varies!)  on reset pin - seems to help with the POR

Filter caps on Vreg

Device is blank - ICP is only automatic on a blank device.

 

For 2)

Are you prompted for a driver when first plugging in?

Check in the hardware manager under windows for the device.  If it doesn't appear at all then it's probably a hardware problem.

If it appears as a unknown device check the properties. It should be reported under "Device Instance Id" as

 USB\VID_0425&PID_FF02\5&12D03F87&0&1
If so, then the device is being recognized correctly and it's a driver problem.  Right-click on the device and re-install the driver from that supplied with the AN2399SW.

 

Not much else to check - It has worked reliably for me under windows-XP SP1, 2 & 3.

 

hope this helps.

 

bye

 

 

 

Message Edited by pgo on 2009-09-21 11:24 AM
0 件の賞賛
返信
1,859件の閲覧回数
nic
Contributor I
Thanks, for your help. I proved all that you tell me but I am not sure about the
conection D+ and D-. bye
Message Edited by nic on 2009-09-21 05:15 PM
0 件の賞賛
返信