Problem with 9S08DZ60 PWM output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with 9S08DZ60 PWM output

2,150 Views
Yang_Guosheng
Contributor I

See the below, This program code of PWM can run EVB9S08DZ60 but we don't generat PWM .
Could you help me check it ?  Could you send me a source code of PWM about EVB9S08DZ60 ?

Thank you very much for you help!

 

#include <hidef.h>
#include "derivative.h" /* include peripheral declarations */

#define   PUSH_PTA4 0
#define   PUSH_PTA5 1
#define   PUSH_PTA6 2
#define   PUSH_PTA7 3

char push;
/////////////////////////////////////////////////////////////////////////////////////////
// PeriphInit
// --------------------------------------------------------------------------------------
// Initializes various registers and peripherals
/////////////////////////////////////////////////////////////////////////////////////////
void PeriphInit(void)
{
   
 // Clear COP Watchdog timeout
 SOPT1 = 0x00;
 
 // Select FBE MCG mode (IREFS=0, CLKS=10)
 MCGC1 = 0xB8;
 // LP=0 and selects external high frequency crystal clock                   
 MCGC2 = 0x36;
 // PLLS=0
 MCGC3 = 0x00;
 // Wait until the initialization cycle of the external crystal clock is completed
 while(!(MCGSC&0x02))
   ;   
 
 //Select fBUS/2 as ADC clock source, clock divide 2 and 8 bit conversion mode
 ADCFG = 0x21;
 
 // Configure PTD port as output and power off LEDs
 PTDD = 0xFF; 
 PTDDD = 0xFF;

 // Enable AD1 and AD2 pins
 APCTL1 = 0x06;
 
 // Enable PTB input pull-downs
 PTBDD = 0x00;
 PTBPS = 0xFF;
 PTBES = 0xFF;
 PTBPE = 0xFF;
 
 
 //tpm1 configure
 TPM1MODH = 0x00;
 TPM1MODL = 0x50;
 TPM1SC = 0x0f;
 
 
 TPM1C0VH = 0x00;
 TPM1C0VL = 0x14;
 TPM1C0SC = 0x14;
 
 //TPM1C0VH = 0x00;
 //TPM1C0VL = 0x14;
 //TPM1C0SC = 0x5a;
 // Enable PTA4, PTA5, PTA6 and PTA7 input pull-ups
 PTAPE = 0xF0;
 
}

/////////////////////////////////////////////////////////////////////////////////////////
// MAIN
/////////////////////////////////////////////////////////////////////////////////////////
void main (void)
{


 
 PeriphInit();
 EnableInterrupts;
 
 push = PUSH_PTA4;
 for(;:smileywink:
 {
   
   
 }   

}

- Mod Corrected Subject line -

Message Edited by Alban on 2007-01-25 01:49 PM

Labels (1)
0 Kudos
Reply
1 Reply

1,127 Views
thisobj
Contributor III

Guosheng,

The following line from your code:
TPM1C0SC = 0x14;

will configure the channel for Output Compare.

To configure for Edge-aligned PWM, the following should work:

TPM1C0SC = 0x28; //=============== for high-true pulses
or
TPM1C0SC = 0x24; //=============== for low-true pulses

I noticed your topic line mentions "9S08GZ60" and your message discusses "9S08DZ60", which I assume is correct, since you stated that you were using the EVB9S08DZ60 board. Please be certain to consult the correct document -- MC9S08DZ60.PDF for the 9S08DZ60. The timer setup differs between these 2 devices.

Frank

- Mod Corrected Subject line according to thisobj obsvervation-

Message Edited by Alban on 2007-01-25 01:49 PM

0 Kudos
Reply