Problem with 13193 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with 13193 EVK

4,139 Views
admin
Specialist II
Hi:
I am a student of UPV(Universidad del Pais Vasco) of spain. I am making the master´s dissertation project related to zigbee. I must to prove the different models from network but I don,t know how make a mesh network.
In smac there is some application that uses this type of network?
Can you tell me that application I must load and how to configure it?
Thanks in advance.
Best regards
Labels (1)
0 Kudos
Reply
3 Replies

1,876 Views
UK_CF_FAE
NXP Employee
NXP Employee

Hello,

With Zigbee we consider 4 main types of networking:

1) Point-to-Point. The SMAC comes with a demo called Wireless UART.mcp which illustrates P2P.

2) Star topology. Here, one main node is the 'hub' of a network with each 'device' connected directly to the hub. The SMAC is capable of Star topology, but does no do this "Out-of-the-Box".  Submit a service request to www.freescale.com/support and ask for the SMAC Star software. This is not supported by Freescale, though, so you'll get no technical support for it. (but post here and we'll try to help you).

3) Cluster Tree. Here, the network is more complex. Each message has only one route across the network, you can think of devices ("leaves" in a tree) passing messages up and down a network, though twigs, branches, trunk, branches, twigs to another device. You'll need the EVK software to demonstrate this. Cluster Tree topology is defined in IEEE802.15.4 at www.ieee.org

4) Mesh. This is the most complex architecture, with any node having more than one route to another device. Zigbee is a networking layer on top of the IEEE layer to support mesh networks. The evaluation of the Zigbee stack at www.freescale.com/zigbee is what you need here.

I should mention a couple of things:

The software packages mentioned above are compiled with CodeWarrior for HC08 Version 3.1, and build up to 60k of flash. The current version of CodeWarrior is version 5.0, so you'll need an older version - 3.1

You wil need a compiler-upgrade licence to 60k to compile the IEEE and Zigbee software. SMAC is is source form, IEEE and Zigbee are library builds.

"Zigbee" is a large and complex topic. You have a very long way to travel, so Good Luck.

Mark

0 Kudos
Reply

1,876 Views
admin
Specialist II
Hello,
I want to use SMAC for create a star network and I have submited a service request as you have suggested, but the only response was to use the MAC codebase, but I must use SMAC because I can't buy a license for Codewarrior.
Can you help me? Thanks a lot!
0 Kudos
Reply

1,876 Views
peg
Senior Contributor IV

Hi,

I believe the SMAC does not do mesh netwowrking. This is one of the reasons for the 'S' in SMAC. "Simple".

Take a look at the Zigbee forum on www.freegeeks.net. I believe this topic is covered there.

Regards Peg

 

0 Kudos
Reply