Prgarmming error of MC9S08GT60

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Prgarmming error of MC9S08GT60

3,391 次查看
praveen
Contributor I

Hi,
please find attachment freescale.bmp
I am trying to program the MC9S08GT60 IC with cyclone pro with
BDM connecter but the following error is shown while programming.

 

I used 9S08GT60.S8P and 9S08GT60A.S8P algorithm file which I used for my programming. I tried with both of them.

 

 

 

Message Edited by praveen on 2007-01-0404:28 AM

Message Edited by praveen on 2007-01-0404:30 AM

标签 (1)
0 项奖励
回复
2 回复数

1,381 次查看
RockyRoad
Contributor III
praveen -
 
I'm trying to work through a similar problem here. I haven't been able to spend the time to completely investigate my problem, but here are some observations that might help you.
 
Peg's hint about the trim value is helpful. The trim value of $00 that the P&E tool is calculating is really wrong. It is likely that the internal oscillator will not actually run with the $00 loaded into the TRIM register. This is why you get the error 14. When the S8P stuffs the the TRIM register with zeroes, the oscillator quits and the rest of the file can't run.
 
This error in calculating the trim has to be due to the tool not reading the sync pulse properly. In my case, I have found that adding 10K external pull-ups to the BKGD pin and the reset pin solve my problem. (You are not supposed to have to use external pull-ups. I'm working on debugging a new S08 and this is probably only a workaround for some other problem specific to the new device. I found this workaround and kept working on other tasks, so I have not gone back to find the root cause yet.)
 
I'm not suggesting that this is the solution for your case. However, you should look at your circuit and make sure that there is not something on the BKGD pin that may be interferring with the P&E tool calculating the correct trim value.
 
- Rocky
0 项奖励
回复

1,381 次查看
peg
Senior Contributor IV
Hi praveen,
 
Firstly, there is no difference between the algorithm files for the GT60 and GT60A!
 
Error 14 is described simply as Error Loading .S8P file. Which you already know.
 
I think the problem is shown a few lines further up. The recommended trim is calculated as zero.
This should not happen and the trim should be calculated even though the device is secure.
Is it really secured?
What is your clock source?
 
Regards
Peg
 
0 项奖励
回复