Power Cycle Dialog

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,194件の閲覧回数
benthie
Contributor II

Hello everybody,

 

I´m working with a MC9S08QB4 at the moment and my problem is, like the topic already said, the "Power Cycle Dialog". CodeWarrior (10.2) is telling me that the MCU is not responding. I´ve done some research about that problem and usually the first idea is to check the BDM-6Pin-Tool-Connector. I did that and have the following question:

 

Pin1 is connected to BKGD (PTA4) and VSS at the same time?

 

Because if I am not totally wrong, that is what the ReferenceManual (Rev.1, page 25) tells me.

 

Thanks and regards,

Ben

ラベル(1)
1 解決策
2,820件の閲覧回数
bigmac
Specialist III

Hello Ben,

The diagram that you refer to is faulty.  Pin 1 of the header is meant to connect to the BKGD/MS pin alone.  Pin 2 connects to ground.

Regards,

Mac

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,820件の閲覧回数
Monica
Senior Contributor III

Hello Ben,

Has this fixed your issue? Don't forget to keep us posted :smileywink:

Best regards,

Monica.

0 件の賞賛
返信
2,820件の閲覧回数
benthie
Contributor II

That has fixed my problem, yes. Sorry for not evaluating the answer. I´m sort of a newbie here :smileywink:

Best regards,

Ben

2,820件の閲覧回数
Monica
Senior Contributor III

No problem, we're happy to have you at Community! :smileygrin:

Great week!

Monica

0 件の賞賛
返信
2,821件の閲覧回数
bigmac
Specialist III

Hello Ben,

The diagram that you refer to is faulty.  Pin 1 of the header is meant to connect to the BKGD/MS pin alone.  Pin 2 connects to ground.

Regards,

Mac

0 件の賞賛
返信