Pin reset of HSC08

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin reset of HSC08

1,902件の閲覧回数
PinresetofHCS08
Contributor I

hello,

It is possible to desable the pin reset\ of the HCS08 by desable a bit of any register, because this pin is very sensitive and even if a make a capacitor to the ground, many times the software reset. I'm sure it's this reset because i displayed the reset status register on an LCD.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,185件の閲覧回数
PinresetofHCS08
Contributor I
I'm using MC9S08GT32A MCUs
0 件の賞賛
返信

1,185件の閲覧回数
celsoken
Contributor V

So you have a dedicated Reset pin, have you placed an external pullup resistor to VDD to enhance EMC susceptibility? FS suggests 4K7.

 

Cheers,

 

Celso

0 件の賞賛
返信

1,185件の閲覧回数
celsoken
Contributor V

You have to tell us what specific microcontroller you are using, most uC do have an option of turning reset into an input port.

 

I suggest you also investigate why the part is reset. Maybe you have EMC problems to solve before.

 

Cheers,

 

Celso

0 件の賞賛
返信