PT60 WDOG in emulation CW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PT60 WDOG in emulation CW

1,828 Views
IlConte
Contributor IV

Dear all, I have a MC9S08PT60, I develop the application with CodeWarrior Development Studio Version: 10.3 and USB Multilink.


feed_watchdog: MACRO

            LDHX #-23038      ;first part of reset sequence (0xA602U)

            STHX WDOG_CNT

            LDHX #-19328      ;second part of reset sequence (0xB480U)

            STHX WDOG_CNT

 

          ENDM


I have inizialized the WDOG with:

ldhx    #$C520          
sthx    WDOG_CNT        
ldhx    #$D928          
sthx    WDOG_CNT        
movx    #$04, WDOG_TOVAL
movx    #$00, WDOG_CS2  
movx    #$80, WDOG_CS1  

cli


mainLoop:

nop

feed_watchdog

bra     mainLoop

 

The problem is when I Suspend the excution and go by step, when execute the sthx WDOG_Cnt instruction the execution goes at random address !!

 

9406_9406.pngpastedImage_3.png

 

After the next 2 step:

 

9411_9411.pngpastedImage_5.png

 

How can i solve this problem ?

 

Thanks

 

Stefano

Labels (1)
0 Kudos
Reply
3 Replies

1,669 Views
pavel_sadek
NXP Employee
NXP Employee

HI

you should never step through these sequences, allways go over and keep this atomic, there is limit of just few bus clks see the related info from ref manual below

Pavel

------------------------

 

23.3.1.2 Refreshing the Watchdog

 

The refresh write sequence is a write of 0xA602 followed by a write of 0xB480 to the

WDOG_CNTH:L registers. The write of the 0xB480 must occur within 16 bus clocks

after the write of 0xA602; otherwise, the watchdog resets the MCU.

 

Before starting the refresh sequence, disable global interrupts.

Otherwise, an interrupt could effectively invalidate the refresh

sequence if writing the four bytes takes more than 16 bus

clocks. Re-enable interrupts when the sequence is finished.

 

23.3.1.3 Example code: Refreshing the Watchdog

 

The following code segment shows the refresh write sequence of the WDOG module.

 

/* Refresh watchdog */

for (;;) // main loop

{

...

DisableInterrupts; // disable global interrupt

WDOG_CNT = 0xA602; // write the 1st refresh word

WDOG_CNT = 0xB480; // write the 2nd refresh word to refresh counter

EnableInterrupts; // enable global interrupt

...

}

0 Kudos
Reply

1,669 Views
larrymitschke
Contributor II

Thanks, Pavel,

Yes, I followed all that religiously, and got an immediate [WDOG, RESET, Illegal Opcode, Illegal Address, etc] interrupt on the first write when I stepped through it.  With the option to enable WDOG in chip debug mode, I assumed stepping through would be OK, especially since the clock source is the bus clk.  I'll take your advice and just run through that process.

Thanks,

lm

0 Kudos
Reply

1,669 Views
larrymitschke
Contributor II

I am having the same problem.

0 Kudos
Reply