PROBLEM WINDOWS VISTA CW 6.2 HIWAVE (DEBUG)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PROBLEM WINDOWS VISTA CW 6.2 HIWAVE (DEBUG)

2,652件の閲覧回数
rodolfo_oliveir
Contributor I

Good morning,

     We install Windows Vista on computers here in the Department of Development of Hardware (Company: Autotrac) and reinstalling the CodeWarrior 6.2, but after performing these tasks, the "True-Time Simulator & Real-Time Debugger" (software debugging) is presenting the message below (Print), after selecting the "Open Source File" to perform the debugging.
     You could help us?

Message: atached picture.

 

Note: The settings are made for Windows XP and everything works smoothly.
 
 
Regards,
Rodolfo Romão de Oliveira Neto
 
Message Edited by t.dowe on 2009-10-27 11:46 AM
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,482件の閲覧回数
J2MEJediMaster
Specialist I

This is a licensing error. Did you download and install a Special Edition of the tools, or the 30-day Evaluation Edition of the tools? If you have paid for the tools, then something happened to your license.dat file. (I see you mentioned reinstalling the software.) If you paid for the tools, then you need to enter a Service Request and report this as a license problem. To do this, click here to go to the Service Request page. On the Service Request page, select Technical Request for the Category and License Issues for the topic. You should provide the entitlement ID or similar supporting purchase information with the Service Request so that they can help you.

 

---Tom

 

0 件の賞賛
返信

1,482件の閲覧回数
rodolfo_oliveir
Contributor I

Good morning,

Yes, my company bought the lincença, already been in contact with Freescale and I believe that experts are examining the issue, the order has already been opened, but not receive an answer, so tried the forum.
My licença.dat is the same as the other engineers use as it is on the server, and they can use it without problems with Windows XP and I can not use with Windows Vista. I think this is the problem because the only difference between the environment is the operating system.

 

 

Regards,

Rodolfo Romão.

0 件の賞賛
返信

1,482件の閲覧回数
J2MEJediMaster
Specialist I

Are you using the 64-bit version of Vista? CodeWarrior for Microcontrollers 6.2 is only compatible with 32-bit Windows Vista.

 

---Tom

0 件の賞賛
返信