PN Check

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN Check

2,641 Views
tradingking
Contributor I

Hi I have a question on MPN that I've found 2 different mpn. 

 

S9S12ZVL96F0MLF  vs S912ZVL96F0MLF  

Please explain what is the difference for these 2 pn. 

 

Thanks.

0 Kudos
Reply
3 Replies

2,597 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

There is only one datasheet for both devices. The differences are mentioned in related chapters.

It can  be found and downloaded at >

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-m...

or....

( S12 MagniV® S12ZVL – Reference Manual    )

 

Best regards,

Ladislav

0 Kudos
Reply

2,630 Views
KalaimaniArumugamdev
Contributor III

HI @tradingking 

              The difference between S9S12ZVL96F0MLF and S912ZVL96F0MLF is memory size. It is mentioned in the datasheet on page number 748 and 749.

Thanks 

Kalaimani Arumugam

0 Kudos
Reply

2,601 Views
tradingking
Contributor I

Can please help me get the datasheet for both S9S12ZVL96F0MLF and S912ZVL96F0MLF ?

Thank you. 

0 Kudos
Reply