PLEASE HELP ME: background mode Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PLEASE HELP ME: background mode Problem

ソリューションへジャンプ
2,613件の閲覧回数
bitasobhani
Contributor III

Hi all

I cannot program 1321x SRB board by a BDM programmer when I use switching power supply (yellow led on programmer is OFF). But when I use USB supply it can be programmed (yellow led on programmer is ON). I have the same problem when programming 13192 SARD board whith switching power supply. Unfortunately the board has no USB connector. So I cannot program the board at all. 

I measured switching power supply voltage with voltmeter. It is 9.15volt.

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,797件の閲覧回数
bitasobhani
Contributor III

Thanks for reply

I solved the problem. It was due to disconnection of the board ground and programmer ground pin in flat cable. So when I used USB supply, the two groud was connected through the computer.

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,797件の閲覧回数
peg
Senior Contributor IV

Hello,

 

Does the SARD board work with a 9V battery?

Does the green power LED on the SARD come on with the external power supply like it does with the battery?

You do realise the power switch works opposite when using external power supply.

Can you measure 3 volts on the 2 pins behind the serial socket? (marked 3V and + -)

 

0 件の賞賛
返信
1,798件の閲覧回数
bitasobhani
Contributor III

Thanks for reply

I solved the problem. It was due to disconnection of the board ground and programmer ground pin in flat cable. So when I used USB supply, the two groud was connected through the computer.

 

0 件の賞賛
返信