P87C51 replacement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P87C51 replacement

1,300 Views
nigelhale
Contributor I

I am looking for a replacement for the now obsolete P87C51SBAA,512 processor.

I have fitted the second generation P87C51MC2BA/02,529 device, programmed with the same .hex file as used for the old part.

I notice in the data sheet for the new part that it runs instructions at twice the speed of the old part

The critical timings in our application make use of Timer 1 so I did not expect them to change.

However, I find that these timings have halved when the code is run in the new part.

Is this because the internal clock runs at twice the speed, resulting in timer time-out periods also being halved?

Tags (1)
0 Kudos
Reply
0 Replies