Overwritten memory; MC9S08AW60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Overwritten memory; MC9S08AW60

Jump to solution
1,932 Views
janr_
Contributor I

Hello,

I try to tesst my programm with the True time simulator.

However after sbufferpos = 15 (after 15 times ISR_Interrupt) some parts of the buffer array will be overwritten.

Then there occurs an error:

Error: At location 0057 -

Error: Attempt to execute from unimplemented (--) ROM

 

Do you have any idea how to fix this problem?

 

// Includes ----------------------------------------------------------------------------------------

#include <hidef.h> /* for EnableInterrupts macro */

#include "derivative.h" /* include peripheral declarations */

#include "SPIDriver.h"

 

 

// Variablen ---------------------------------------------------------------------------------------

static volatile int sbufferpos = 0;

byte buffer[33];

 

// Prototypen --------------------------------------------------------------------------------------

void BefehlsbufferErstellen(int takt);

void SendeBuffer(byte b);

 

// Main --------------------------------------------------------------------------------------------

void main(void) {

 

 

 

      spi_init();

      spi_setMode(Master, FallingEdge, LeadingEdge, MSBfirst);

    spi_selectChip(true,0);

    BefehlsbufferErstellen(27);

      spi_enableInterrupt(true);

 

      for(;;)

        {    

            __RESET_WATCHDOG();

        } 

   }

 

 

// Interruptroutinen ---------------------------------------------------------------------------------

__interrupt VectorNumber_Vspi1 void ISR_SPI() {

   

           if((SPI1S&(SPI1S_SPRF_MASK)) == 0) {

           }

           else{

              SPI1S;

              SPI1D;

           }

           if((SPI1S&(SPI1S_SPTEF_MASK)) == 0){ 

           }

           else{

                spi_enableInterrupt(false);

                if(sbufferpos > sizeof(buffer) - 1) {

                 sbufferpos = 0;

                } else{

                SendeBuffer(buffer[sbufferpos]);

                sbufferpos++;

                spi_enableInterrupt(true);

                }

            }

}

 

// Funktionen -----------------------------------------------------------------------------------------

void BefehlsbufferErstellen (int takt) {

 

 

  if(takt== 27) {

 

  buffer[0]= 0x9F;    // Set Address

  buffer[1]= 0x24;    // 36d

  buffer[2]= 0x40;    // Write

  buffer[3]= 0x4F;    // 4Fh

 

  buffer[4]= 0x9F;    // Set Address

  buffer[5]= 0x28;    // 40d

  buffer[6]= 0x40;    // Write

  buffer[7]= 0x00;    // 00h

 

  buffer[8]= 0x9F;    // Set Address

  buffer[9]= 0x29;    // 41d

  buffer[10]= 0x40;   // Write    

  buffer[11]= 0x02;   // 02h

 

  buffer[12]= 0x9F;   // Set Address

  buffer[13]= 0x30;   // 42d

  buffer[14]= 0x40;   // Write    

  buffer[15]= 0x9F;   // 0x9Fh

 

  buffer[16]= 0x9F;   // Set Address

  buffer[17]= 0x32;   // 44d

  buffer[18]= 0x40;   // Write    

  buffer[19]= 0x00;   // 00h

 

  buffer[20]= 0x9F;   // Set Address

  buffer[21]= 0x33;   // 45d

  buffer[22]= 0x40;   // Write    

  buffer[23]= 0x0D;   // 0Dh

 

  buffer[24]= 0x9F;   // Set Address

  buffer[25]= 0x35;   // 47d

  buffer[26]= 0x40;   // Write    

  buffer[27]= 0x00;   // 00h

 

  buffer[28]= 0x9F;   // Set Address

  buffer[29]= 0x36;   // 48d

  buffer[30]= 0x40;   // Write    

  buffer[31]= 0x0D;   // 0Dh

 

 

  }

  else if(takt == 26){

 

  buffer[0]= 0x9F;    // Set Address

  buffer[1]= 0x24;    // 36d

  buffer[2]= 0x40;    // Write

  buffer[3]= 0x3D;    // 3Dh

 

  buffer[4]= 0x9F;    // Set Address

  buffer[5]= 0x28;    // 40d

  buffer[6]= 0x40;    // Write

  buffer[7]= 0x20;    // 20h

 

  buffer[8]= 0x9F;    // Set Address

  buffer[9]= 0x29;    // 41d

  buffer[10]= 0x40;   // Write    

  buffer[11]= 0x95;   // 95h

 

  buffer[12]= 0x9F;   // Set Address

  buffer[13]= 0x30;   // 42d

  buffer[14]= 0x40;   // Write    

  buffer[15]= 0xFF;   // FFh

 

  buffer[16]= 0x9F;   // Set Address

  buffer[17]= 0x32;   // 44d

  buffer[18]= 0x40;   // Write    

  buffer[19]= 0x03;   // 03h

 

  buffer[20]= 0x9F;   // Set Address

  buffer[21]= 0x33;   // 45d

  buffer[22]= 0x40;   // Write    

  buffer[23]= 0xE8;   // E8h

 

  buffer[24]= 0x9F;   // Set Address

  buffer[25]= 0x35;   // 47d

  buffer[26]= 0x40;   // Write    

  buffer[27]= 0x03;   // 03h

 

  buffer[28]= 0x9F;   // Set Address

  buffer[29]= 0x36;   // 48d

  buffer[30]= 0x40;   // Write    

  buffer[31]= 0xE8;   // E8h

 

  }

  else {

  }

}

 

 

void SendeBuffer(byte b) {

 

__RESET_WATCHDOG();

spi_sendData(b);

 

}

Labels (1)
0 Kudos
Reply
1 Solution
1,691 Views
bigmac
Specialist III

Hello,

These symptoms would indicate a stack overflow problem.  It may be possible that you have an unintended nested interrupt situation.  The spi_enableInterrupt() function might be a possible cause, if it is globally enabling interrupts within the ISR function.  The use of this function within the ISR would seem unnecessary, except for the final disable of the SPI interrupt when the data sequence is completed.  I would also suspect that you have the SPTEF interrupt enabled, which will exacerbate the problem.

If you wish to use interrupts for SPI master operation, only the RDRF interrupt should be enabled - the SPTEF interrupt should remain disabled.  When the RDRF flag becomes set, this means that the transfer of the last send byte has been completed, and the next byte may now be sent after the RDRF flag has been cleared.  It is not necessary to test the SPTEF flag.

I assume that the spi_selectChip() function is simply enabling the CS signal to the external device.  You do not appear to be disabling the signal after completion of the send sequence.  Since the data sequence is loaded byte-by-byte into the array variable, this would seem very inefficient.  An alternative method would be to create constant array variables directly within flash memory.  The data can then be accessed using a pointer variable, without the need for using an array variable.  The following code snippet shows this approach.

//-----------------------------------------------------------------------------
// Global variables:

volatile byte *pntr;
volatile byte buf_count;

//-----------------------------------------------------------------------------
// Data sequence tables:

const byte data_seq1[] = {
  0x9F, 0x24, 0x40, 0x4F,
  0x9F, 0x28, 0x40, 0x00,
  0x9F, 0x29, 0x40, 0x02,
  0x9F, 0x30, 0x40, 0x9F,
  0x9F, 0x32, 0x40, 0x00,
  0x9F, 0x33, 0x40, 0x0D,
  0x9F, 0x35, 0x40, 0x00,
  0x9F, 0x36, 0x40, 0x0D
};

const byte data_seq2[] = {
  0x9F, 0x24, 0x40, 0x3D,
  0x9F, 0x28, 0x40, 0x20,
  0x9F, 0x29, 0x40, 0x95,
  0x9F, 0x30, 0x40, 0xFF,
  0x9F, 0x32, 0x40, 0x03,
  0x9F, 0x33, 0x40, 0xE8,
  0x9F, 0x35, 0x40, 0x03,
  0x9F, 0x36, 0x40, 0xE8
};

//-----------------------------------------------------------------------------

void main(void)
{
  SPI_init();
  EnableInterrupts;             // Globally enable interrupts

  SPI_selectChip( true, 0);     // Enable SPI slave device
  SPI_send_start( 27);          // Start send sequence
  while (buf_count)             // Wait until send sequence completed
    __RESET_WATCHDOG();
  SPI_selectChip( false, 0);    // Disable SPI slave device
 
  for( ; ; )  {    
    __RESET_WATCHDOG();

  } 
}

//-----------------------------------------------------------------------------
// Start SPI send sequence

void SPI_send_start( byte takt)
{
  if (takt == 27)  pntr = data_seq1;
  if (takt == 26)  pntr = data_seq2;
  if (takt) {
    while (SPI1S_SPTEF == 0);
    SPI1D = *pntr++;            // Send first byte of sequence
    buf_count = 31;
    SPI_Interrupt( true);       // Enable SPRF interrupts
  }
  else  buf_count = 0;
}

//-----------------------------------------------------------------------------
// Interrupt functions:

__interrupt VectorNumber_Vspi1
void ISR_SPI( void)
{
  (void)SPI1S;                  // Clear SPRF flag
  (void)SPI1D;

  if (buf_count) {
    SPI1D = *pntr++;
    buf_count--;
  }
  else
    SPI_Interrupt( false);      // Disable SPI interrupts
}

Regards,

Mac

View solution in original post

0 Kudos
Reply
2 Replies
1,692 Views
bigmac
Specialist III

Hello,

These symptoms would indicate a stack overflow problem.  It may be possible that you have an unintended nested interrupt situation.  The spi_enableInterrupt() function might be a possible cause, if it is globally enabling interrupts within the ISR function.  The use of this function within the ISR would seem unnecessary, except for the final disable of the SPI interrupt when the data sequence is completed.  I would also suspect that you have the SPTEF interrupt enabled, which will exacerbate the problem.

If you wish to use interrupts for SPI master operation, only the RDRF interrupt should be enabled - the SPTEF interrupt should remain disabled.  When the RDRF flag becomes set, this means that the transfer of the last send byte has been completed, and the next byte may now be sent after the RDRF flag has been cleared.  It is not necessary to test the SPTEF flag.

I assume that the spi_selectChip() function is simply enabling the CS signal to the external device.  You do not appear to be disabling the signal after completion of the send sequence.  Since the data sequence is loaded byte-by-byte into the array variable, this would seem very inefficient.  An alternative method would be to create constant array variables directly within flash memory.  The data can then be accessed using a pointer variable, without the need for using an array variable.  The following code snippet shows this approach.

//-----------------------------------------------------------------------------
// Global variables:

volatile byte *pntr;
volatile byte buf_count;

//-----------------------------------------------------------------------------
// Data sequence tables:

const byte data_seq1[] = {
  0x9F, 0x24, 0x40, 0x4F,
  0x9F, 0x28, 0x40, 0x00,
  0x9F, 0x29, 0x40, 0x02,
  0x9F, 0x30, 0x40, 0x9F,
  0x9F, 0x32, 0x40, 0x00,
  0x9F, 0x33, 0x40, 0x0D,
  0x9F, 0x35, 0x40, 0x00,
  0x9F, 0x36, 0x40, 0x0D
};

const byte data_seq2[] = {
  0x9F, 0x24, 0x40, 0x3D,
  0x9F, 0x28, 0x40, 0x20,
  0x9F, 0x29, 0x40, 0x95,
  0x9F, 0x30, 0x40, 0xFF,
  0x9F, 0x32, 0x40, 0x03,
  0x9F, 0x33, 0x40, 0xE8,
  0x9F, 0x35, 0x40, 0x03,
  0x9F, 0x36, 0x40, 0xE8
};

//-----------------------------------------------------------------------------

void main(void)
{
  SPI_init();
  EnableInterrupts;             // Globally enable interrupts

  SPI_selectChip( true, 0);     // Enable SPI slave device
  SPI_send_start( 27);          // Start send sequence
  while (buf_count)             // Wait until send sequence completed
    __RESET_WATCHDOG();
  SPI_selectChip( false, 0);    // Disable SPI slave device
 
  for( ; ; )  {    
    __RESET_WATCHDOG();

  } 
}

//-----------------------------------------------------------------------------
// Start SPI send sequence

void SPI_send_start( byte takt)
{
  if (takt == 27)  pntr = data_seq1;
  if (takt == 26)  pntr = data_seq2;
  if (takt) {
    while (SPI1S_SPTEF == 0);
    SPI1D = *pntr++;            // Send first byte of sequence
    buf_count = 31;
    SPI_Interrupt( true);       // Enable SPRF interrupts
  }
  else  buf_count = 0;
}

//-----------------------------------------------------------------------------
// Interrupt functions:

__interrupt VectorNumber_Vspi1
void ISR_SPI( void)
{
  (void)SPI1S;                  // Clear SPRF flag
  (void)SPI1D;

  if (buf_count) {
    SPI1D = *pntr++;
    buf_count--;
  }
  else
    SPI_Interrupt( false);      // Disable SPI interrupts
}

Regards,

Mac

0 Kudos
Reply
1,691 Views
weapon
Senior Contributor I

Hi

I didn't see any problem in your code. could you provide the whole project to me?  I'd like to check the PRM file and MAP file.

Best Regards

XWP

0 Kudos
Reply