OrCad footprint Library file for MC9S08AW60CPUE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OrCad footprint Library file for MC9S08AW60CPUE

5,792 次查看
TomT
Contributor I
Would anyone happen to have the library file for this part in their OrCad library? I do not have the time to create a new part and I am sure that somone has already done this.
Please email me the file at [email protected] if you wouldn't mind.
 
Very much appreciated...thanks.
 
标签 (1)
0 项奖励
回复
4 回复数

1,874 次查看
Alban
Senior Contributor II
Good Evening,
 
Generally speaking post in which the author is asking a reply by email are very likely to be ignored.
A forum is about exchange and replies by emails are only a one way street.
 
Furthermore, if the author is not willing to come back to the forum to read the answer to his questions, Contributors are likely not to be willing to waste time in answering.
 
Finally, this Forum has the possibility to subscribe to a thread and receive email notification (with the body of the message) of any reply being posted.
That is a more subtle way to secure an answer via email without showing lack of interest in the community principles.
 
Kind Regards,
Alban.
0 项奖励
回复

1,874 次查看
yb
Contributor IV
Hi,
Create a component like this take 10 minutes...
 
Yvan
0 项奖励
回复

1,874 次查看
Kender
Contributor I
You might be able to find the OrCAD library in this yahoo group:

Message Edited by Kender on 2007-04-0504:16 AM

Message Edited by Kender on 2007-04-0504:16 AM

0 项奖励
回复

1,874 次查看
Alban
Senior Contributor II

Hi, MC9S08AW60CPUE is not a 16-Bit product and message was moved to appropriate board.
Alban.

0 项奖励
回复