OrCad footprint Library file for MC9S08AW60CPUE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OrCad footprint Library file for MC9S08AW60CPUE

5,793件の閲覧回数
TomT
Contributor I
Would anyone happen to have the library file for this part in their OrCad library? I do not have the time to create a new part and I am sure that somone has already done this.
Please email me the file at [email protected] if you wouldn't mind.
 
Very much appreciated...thanks.
 
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,875件の閲覧回数
Alban
Senior Contributor II
Good Evening,
 
Generally speaking post in which the author is asking a reply by email are very likely to be ignored.
A forum is about exchange and replies by emails are only a one way street.
 
Furthermore, if the author is not willing to come back to the forum to read the answer to his questions, Contributors are likely not to be willing to waste time in answering.
 
Finally, this Forum has the possibility to subscribe to a thread and receive email notification (with the body of the message) of any reply being posted.
That is a more subtle way to secure an answer via email without showing lack of interest in the community principles.
 
Kind Regards,
Alban.
0 件の賞賛
返信

1,875件の閲覧回数
yb
Contributor IV
Hi,
Create a component like this take 10 minutes...
 
Yvan
0 件の賞賛
返信

1,875件の閲覧回数
Kender
Contributor I
You might be able to find the OrCAD library in this yahoo group:

Message Edited by Kender on 2007-04-0504:16 AM

Message Edited by Kender on 2007-04-0504:16 AM

0 件の賞賛
返信

1,875件の閲覧回数
Alban
Senior Contributor II

Hi, MC9S08AW60CPUE is not a 16-Bit product and message was moved to appropriate board.
Alban.

0 件の賞賛
返信