OLD: Painter / UOC Bench Programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OLD: Painter / UOC Bench Programmer

975 Views
r_christopherlo
Contributor I


This almost belongs in a historical forum, but here goes.  I foolishly threw away my two bench programmers a few years ago during an office move.  At the time, it seemed I would NEVER need them again.  Well, guess what?  I received a small order for an old Painter-based product.  I can still get blank Painter chips, but without a programmer I'm out of luck. 

 

To the best of my knowledge, these units were never sold, but were clearly provided to each development team for lab testing.  The part number for the two units I had are as follows:

 

7313 903 0024-3 Painter/UOC Bench Programmer

 

 

7313 903 0024-2  Painter/UOC Bench Programmer

 

Note: the “903” could be “303” or “503”, I can’t tell exactly from the picture I have.  They function identically, just the -3 version is slightly newer one.  The two I had were made out of the Southampton office, and my contact there told me all remaining equipment had been purged years ago with the cancellation of the Painter / UOC family. 

 

Alternatively, if someone knows whether Philips/NXP ever released the programming details for these chips, I could consider "rolling my own" programmer.  That would depend on the details, of course.

 

Help much appreciated.

 

-Chris Lott

Seoul, South Korea

Labels (1)
0 Kudos
Reply
0 Replies