No rule to make target error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No rule to make target error

1,637件の閲覧回数
andresfelipecas
Contributor II

hi, I made a program using codewarrior 10.4. when I updated to 10.6 the projects made by 10.4 show an error which says like this: mingw32-make.***No rule to make target..... and then it shows that the program cant load hidef.h because the path is with the codewarrrior 10.4 folder. when y change the codewarrior 10.6 folder name by 10.4 the error don't ever show up. I want to correct this problem without changing the folder name.

ラベル(1)
0 件の賞賛
返信
1 返信

1,066件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Pipe,

please pay attention to this point:

1. CW10.4 and CW10.6 can't share the same workspace folder

2. before build , go to menu "project", "clean...". to clean up the old associations. then rebuild the project.

========================================

this answer is for you. if it helps, please click on "correct answer " button.

Best Regards,

ZhangJun

0 件の賞賛
返信