Newbies: .S19 file and program mode!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Newbies: .S19 file and program mode!

1,699 Views
Ciccio
Contributor I
Hi,
I am newbies!
If I want program my MC9S08AW44 with file .S19 whitout use debug mode, with only file object, How I do it?
I have not the source!
Thanks
Labels (1)
0 Kudos
Reply
1 Reply

1,153 Views
peg
Senior Contributor IV
Hi Ciccio,
 
Run Hiwave.exe which is located in the prog directory under your CW installation directory.
From the component menu select the Set Connection...
In here select device type and connection type.
Under the menu labelled by your connection type select the exact device.
Now connect to the device.
Now again under the menu select load...
In here you can select the s19 file and off you go!
 
0 Kudos
Reply