Newbies: .S19 file and program mode!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Newbies: .S19 file and program mode!

1,712 次查看
Ciccio
Contributor I
Hi,
I am newbies!
If I want program my MC9S08AW44 with file .S19 whitout use debug mode, with only file object, How I do it?
I have not the source!
Thanks
标签 (1)
0 项奖励
回复
1 回复

1,166 次查看
peg
Senior Contributor IV
Hi Ciccio,
 
Run Hiwave.exe which is located in the prog directory under your CW installation directory.
From the component menu select the Set Connection...
In here select device type and connection type.
Under the menu labelled by your connection type select the exact device.
Now connect to the device.
Now again under the menu select load...
In here you can select the s19 file and off you go!
 
0 项奖励
回复