Newbies: .S19 file and program mode!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Newbies: .S19 file and program mode!

1,675件の閲覧回数
Ciccio
Contributor I
Hi,
I am newbies!
If I want program my MC9S08AW44 with file .S19 whitout use debug mode, with only file object, How I do it?
I have not the source!
Thanks
ラベル(1)
0 件の賞賛
返信
1 返信

1,129件の閲覧回数
peg
Senior Contributor IV
Hi Ciccio,
 
Run Hiwave.exe which is located in the prog directory under your CW installation directory.
From the component menu select the Set Connection...
In here select device type and connection type.
Under the menu labelled by your connection type select the exact device.
Now connect to the device.
Now again under the menu select load...
In here you can select the s19 file and off you go!
 
0 件の賞賛
返信