New microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

New microcontroller

4,819件の閲覧回数
CarlosH
Contributor I
I'd like to use the most reclently launched Freescale 8-bit MCU. My project uses 68HC908QY4. What's Freescale 8-bit can i use?
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,623件の閲覧回数
Lundin
Senior Contributor IV
I would recommend you to use S08 if possible. BDM is so much better than the HC08 monitor mode crap and will most likely save you lots of troubleshooting. Especially if you are using a 8-pin device like QT4 where you are forced to adapt your whole design to suit the monitor crap.
0 件の賞賛
返信

2,623件の閲覧回数
irob
Contributor V
I would agree that the HCS08 family is a dream to develop on compared to the MON08 parts. But do yourself a favor (if you switch) and read this thread!

It will save you a bunch of hair-pulling when it happens to you.
0 件の賞賛
返信

2,623件の閲覧回数
tequila
Contributor I
QB8/QB4 havea similar pin layout, but I'm not sure if that's what you want.
0 件の賞賛
返信

2,623件の閲覧回数
joerg
Contributor II
Hi CarlosH

Depending on the supply voltage you could use QB8/4 or QD4 using 3V.
If 5V is a concern you may use a AW16/... device.

Saluti Joerg
0 件の賞賛
返信