New Freescale Offering

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

New Freescale Offering

7,279 Views
BobMac
Contributor I
I just saw the announcement of an extended version of our 'ol faithful, the 908JL8. The 'JL16 has arrived in good time. We are getting a bit "thin" in the flash rom department in regards to a few products now out. I wonder when some documentation will be placed on the web site.
Regards, Bob and the guys
Labels (1)
0 Kudos
Reply
5 Replies

2,453 Views
RockyRoad
Contributor III

Bob -

I don't know why a search doesn't turn it up and why it's not in the product links on the left side of the 8-bit home page, but I did find it all through the link in the announcement:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=68HC908JL16&nodeId=016246844976630196...

Specifically, the data sheet is at:

http://www.freescale.com/files/microcontrollers/doc/data_sheet/MC68HC908JL16.pdf

Hopefully, they'll get the links up soon.

0 Kudos
Reply

2,453 Views
AJC78
Contributor I
Did anybody test this JL16 MCU´s ? , i´ve got some samples and i can´t connect to the module, i used the same kit that y used with JL3/JL8 and the JL16 didn´t connect.
Help please!
0 Kudos
Reply

2,453 Views
soac
Contributor I
FREESCALE IS NUMBER ONE.
 
JUST FINISHED.
 
2 MONTHS FROM CONCEPT TO PRODUCT.
 
YESS!! GREAT!! BEAT THAT???
 
AND IT WORKS.......
 
0 Kudos
Reply

2,452 Views
BobMac
Contributor I
Hey, Thanks Rocky R.!
As you might have supposed, we found it right after my post. A bit of Murphy's law in action. I must be getting blinder than I thought. The update looks quite nice, 16K and a 10 bit ADC brings a bit more to the party 'eh.
Regards, Bob
0 Kudos
Reply

2,452 Views
AJC78
Contributor I

Dear Friends:   Have you got the flash programming algorothm for the JL16 ? (for the P & E Micro IDE)

Thanks a lot!

0 Kudos
Reply