Need to program MC68HC908AS32ACFN - Desperately need help!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need to program MC68HC908AS32ACFN - Desperately need help!

2,185件の閲覧回数
mikev
Contributor I

I have a bunch of MC68HC908AS32ACFN MCU's I need to program for a product line we have acquired. I'm very late on the project. This is new to me. I'm more of a programmer than an electrician. I have the latest Codewarrior for the HC08. I just need to get the code on the chips. I have a P&E 68HC08 MONO8 device, but thats only half the solution. I've tried to wire it to a chip socket... but not doing to well. Is there a 52-pin PLCC adapter that will accept the above MCU and a MONO8 header? Or a complete all-in-one board setup? Almost everything I see out there are for 64-pin QFP versions.

Thank you,

Mike

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,246件の閲覧回数
bigmac
Specialist III
Hello Mike,
 
According to the MON08 Multilink manual, the following connections to the MON08 16-pin header are required for programming the HC908AS -
Pin 2 = Gnd (Vss)
Pin 4 = Reset
Pin 6 = IRQ (Vtst)
Pin 10 = PTA0
Pin 12 = PTC0
Pin 13 = Osc1
Pin 14 = PTC1
Pin 15 = Vout (Vdd)
Pin 16 = PTC3
 
All other pins on the header are not connected.
 
You will need to identify the pins on the PLCC52 that correspond to these connections, and connect accordingly.  I would use a through-hole type PLCC socket for more convenient point-to-point hand wiring.
 
I assume you need to program the devices separately, rather than in situ on the board.
 
Regards,
Mac
 

Message Edited by bigmac on 2007-04-2501:25 PM

0 件の賞賛
返信

1,246件の閲覧回数
rocco
Senior Contributor II
0 件の賞賛
返信