Need help,MC3PHAC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help,MC3PHAC

2,869 Views
sunny
Contributor I
I made a A/C motor drive board with MC3PHAC. The motor's rating is 220V/750W. Now the question is, when the motor runs at high speed(3000rpm/50Hz), everything is ok, but when it runs at 500rpm or slower, both the igbts and the motor become very hot. I don't know why? Can someone help me? Thanks!
Labels (1)
0 Kudos
Reply
2 Replies

1,485 Views
nedemek
Contributor I
Can u send schematic? or attach here?
0 Kudos
Reply

1,485 Views
poornirohit
Fresh Out Contributor

Hi,

please help me i got stucked in sending the commands to mc3phac.it is not responding anything.

please help me........

thanks,

Poornima

0 Kudos
Reply