Multilink 2.0 Does not work wit CodeWarrior 10.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multilink 2.0 Does not work wit CodeWarrior 10.7

1,574件の閲覧回数
monroy39
Contributor I

Operating System: Windows 10 64-bit

I installed drivers for DEMO9S08QG8. Windriver and USB Multilink 2.0 appears
without problems, I mean Windows shows that device is working correctly.

When I tried to connect with Codewarrior 10.7 (at 2016 I can use the Demoboard
without troubles), the IDE cannot recognize the connection.

I download Update Firmware Multilink from P&E site and also not recognize the
connection.

I attached pdf files where I show you that happens with CW 10.7.

First I used the P&E drivers 12.7 (the last release), then I used the 12.3
version.

Installed CW 10.7 and P&E Drivers 12.3 with compatibility W8.

I used W10 at 64bits.

Also I attached a note at 2016, when I had troubles for prog. only is in
spanish because was only for me like a log.

I hope so you can help me.

タグ(1)
0 件の賞賛
返信
1 返信

1,559件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi 

What multilink are you using?

depending the multilink that you have, in some version there are 2 led on in, one is for the multilink power, the second is on when the multilink detect the board (target)

I have win 10  64bit and the USB universal multilink is working without problems

 

Please let me know your comments

Regards

Vicente

 

0 件の賞賛
返信