Monitor  HC908q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Monitor  HC908q

5,317 Views
chempi
Contributor I
Hi everyone
 
I recently bought a HC908qy4, And I made a circuit to get the monitor mode following the AN2305 and 2317 application note.
 
I could achieve the connection between the Pemicro software and the hc908qy4, but I after I programmed the micro, i could not achieve the connection again, I checked and rechecked the connection, but i could not achieve anything, but when I replace de Vtst voltage from the max232 and zener diode (9.1V) with an external source of Vtst (lm78l08) I get the connection again.
 
I don´t understand what this happen, I someone can help me, I would appreciate it
Andres
Labels (1)
0 Kudos
Reply
2 Replies

1,795 Views
eckhard
Contributor V

Hello,

 

the blank chip is using the forced monitor mode, there is no high voltage needed on IRQ.

The programmed chips need Vtst apllied on the IRQ Pin. Sometimes the problem is that the voltage of the MAX232 charge pump is rising too slow to get Vtst applied early enough in the reset sequence. A workaround is to put a delay into Power on Reset. You can do that by keeping a reset button pushed or by adding a RC combination to the reset pin. This works fine for me.

 

Eckhard

0 Kudos
Reply

1,795 Views
yb
Contributor IV

Hi,

Try a 8.2V zener to replace your 9.1V.

The MAX232 deliver sometimes less than 10V.

 

Regards,

Yvan

0 Kudos
Reply