Modify BeeKit code?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Modify BeeKit code?

3,027 次查看
GaryOlmstead
Senior Contributor I
I need to have a full ZIgBee stack (not SMAC), but I am thinking about hardware other than the MC1321x series.  Is it possible to modify the BeeKit stack to accomodate a different transceiver?
 
Gary Olmstead
Toucan Technology
Ventura CA
 
标签 (1)
0 项奖励
回复
3 回复数

1,761 次查看
addiyi
NXP Employee
NXP Employee
Hello Gary,

Using BeeKit and BeeStack codebase, you can select the type of transceiver:  MC1319x, MC1320x or MC1321x. This property is only used when the Target hardware is set to User defined target configuration from Platform menu.

Regards,
Adrian
0 项奖励
回复

1,761 次查看
peg
Senior Contributor IV
Hi Gary,

I believe the license precludes this (must be used with Freescale hardware).


0 项奖励
回复

1,761 次查看
GaryOlmstead
Senior Contributor I
I can't find the license agreement; but it is certainly not possible from the BeeKit.  Guess I'll have to go to Plan B.
 
Thanks for your help.
0 项奖励
回复