Minimum Amplitude of the External Clock Input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minimum Amplitude of the External Clock Input

1,818 Views
jiunnyang
NXP Employee
NXP Employee

As we know the PB is 5V system MCU, and the SU is also high operating voltage(4.5~18v).

How minimum amplitude of the external clock input for the MC9S08PB8VTG and MC9S08SU8?

is there okay for 3.3v OSC?

I can not find these parameters in Datasheet.

Thanks!

Tags (2)
0 Kudos
Reply
1 Reply

1,747 Views
xuan_wu
NXP Employee
NXP Employee

Hi Jiunn,

You can find these parameters in the table: DC characteristics in S08PB/S08SU datasheet.

pastedImage_1.png

As shown in the above table, the minimum amplitude of external clock input can be calculated by the marked formula.

1. The voltage: Vddx = 5V,  the minimum high voltage of the pin: 0.70 x 5v = 3.5V,   3.3V OSC is not OK.

2. The 3.3V OSC is ok only if Vddx <=4.7V.

Thanks 

0 Kudos
Reply