Memory display in debug window CW 11.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory display in debug window CW 11.1

Jump to solution
17,242 Views
Mei
Contributor IV
Hallo Community
After reset perspective in the debug window,
I can no longer select the start address for the memory display
in the memory window at the top right.
Can you help me?
With best regards
Gerd
0 Kudos
Reply
1 Solution
17,027 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Please try to open the old project from codewarrior but using your new workspace, if the project still does not show the memory option, then my recommendation is create a new project and copy all the file from your old project to the new one

Regards

 

View solution in original post

13 Replies
17,214 Views
Mei
Contributor IV
Yes, that's the best.
To the left of the window with the memory locations and their contents, I had the option of entering different
starting addresses for looking at the memory. This happened in a small window.
Best regards
Gerd
 

 

0 Kudos
Reply
17,207 Views
vicentegomez
NXP TechSupport
NXP TechSupport

I am not sure if you want to add memory monitor?

 

 

vicentegomez_1-1670446957321.png

 

0 Kudos
Reply
17,190 Views
Mei
Contributor IV

Yes, I would like to enter a memory address with +. This option is missing on my window.

0 Kudos
Reply
17,187 Views
vicentegomez
NXP TechSupport
NXP TechSupport

please do a clean on your project, and compile it again

 

the other option is that you add a new memory view

vicentegomez_0-1670540716525.png

 

I hope this will help you

 

0 Kudos
Reply
17,173 Views
Mei
Contributor IV

I'm sorry, the error has not been eliminated.
Clicking on "New memory" gives the same memory window as before.
Maybe a more detailed description of the situation will allow us
to fix the error:
- In my Memory Debug window, I'm missing the small "Monitor Memory" window as shown in your picture (see below) or with some projects no memory window appears at all.
- The CW debug function works otherwise without errors.
- Thes errors occur in all projects. (see Startfenster 2.jpg)
- A long time before that, the system worked without errors. The cause could be a crash, the switching off the PC without shutting down.

Now i saw - maybe a solution:
The basis, the mother of all my projects comes from "HS08 Example Projects".
Now this project is missing from the folder. (Image "HCS08 Examples.jpg".There was a line under "mc9s08qg4" before.

Maybe you can send me this example project - mc9s08qg8 - and fix the error with it.

I'm worried that I'll have to go back a long way to fix the error that my carelessness caused.

With best regards

Gerd

0 Kudos
Reply
17,061 Views
vicentegomez
NXP TechSupport
NXP TechSupport

I will send it in a direct email

0 Kudos
Reply
17,034 Views
Mei
Contributor IV

Dear Vicente,

I unzipped the file you sent and pasted it into the CW demos gap. It was possible to import the obtained mc9s08qg8_demo from the CW Examples normally. The debug function is normal, but this time there was no display of the memory table at all. The window is empty, white.

The problem seems to be a brain teaser. I want to write down the facts, maybe that will help.
0. 
All my assembler projects are derived from mc9s08qg8_demo and they worked fine until recently.
1. The virgin new demo project does not show proper normal display of memory
2. 
There are two types of projects. The debug function works normally for all of them.
3. 
The "better" project group displays the memory contents normally, but does not  allow entering a start address. These are older projects.
4. The "bad" project group does not show the memory content at all. 

What should I do?

With best regards

Gerd

 

 

0 Kudos
Reply
17,029 Views
vicentegomez
NXP TechSupport
NXP TechSupport

maybe your workspace is damaged, please create a new one,

 

Regards

0 Kudos
Reply
17,023 Views
Mei
Contributor IV

Dear Vicente,
Yes, that's what I feared. This means I need to re-download CodeWarrior for MCU Version: 11.1. 

But I'm a little afraid of it. Is there a little guide for this? I have to delete the existing CW 11.1, how?
My PC has Windows 11 Home, 64 bit.

Regards
Gerd

0 Kudos
Reply
17,019 Views
vicentegomez
NXP TechSupport
NXP TechSupport

no, first try to create a new folder for a new workspace, when you launch codewarrior you need to create a new folder 

vicentegomez_1-1671039169388.png

 

vicentegomez_0-1671039126403.png

 

 

0 Kudos
Reply
17,017 Views
Mei
Contributor IV

Dear Vicente,
It's done. The memory display and the possibility to enter memory start addresses work with the imported mc9s08qg8_demo. Now can I import my old projects from the backup folders? Could this be the old problem again?

Best wishes from Gerd, who is happy.

Accept as solution and kudos follow.

0 Kudos
Reply
17,028 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Please try to open the old project from codewarrior but using your new workspace, if the project still does not show the memory option, then my recommendation is create a new project and copy all the file from your old project to the new one

Regards

 

17,215 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry, I did not get your question properly can you please send me a picture?

regards

Vicente

0 Kudos
Reply