Medical Applications USB Stack FAQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Medical Applications USB Stack FAQ

12,617 Views
MedicalApplicat
Contributor III

Q:   What is “Medical Applications USB stack”?

A:   Freescale’s Medical Applications USB stack is based on USB's Personal Health Care Device Class PHDC and IEEE-11073 and is compatible with Continua Host emulator software. This Medical USB stack enables microcontrollers with guidelines for Continua Health Alliance connectivity (http://www.continuaalliance.org/) and is a first step to test your application prior official Continua Certification.

Labels (1)
0 Kudos
Reply
12 Replies

7,954 Views
MedicalApplicat
Contributor III

A:   As of September 2009 the Flexis JM demonstration board (DEMOJM) and 9S08JS16 demo board (DEMO9S08JS16) support the Medical Applications USB stack.  The stack is planned to be available for demo and evaluation boards in the future.

0 Kudos
Reply

7,954 Views
MedicalApplicat
Contributor III

A:   As of September 2009 the featured documentation is a step-by-step User Guide (document S08CFV1USBUG) to get you running in short time and a comprehensive reference manual (document S08CFV1USBAPIRM). Application notes and trainings will be supplied soon.

0 Kudos
Reply

7,954 Views
Tacho57
Contributor I

Hi, I search for this documents ... but can't find it, please tell me where to look for. Many Thanks

0 Kudos
Reply

7,954 Views
MedicalApplicat
Contributor III

A:   As of September 2009 the 8-bit 9S08JS16, 9S08JM16, 9S08JM60 and 32-bit  MCF51JM128 support the Medical Applications USB stack. The stack is planned to be available for other 32-bit ColdFire MCUs in the future.

Message Edited by Medical Applications USB Stack on 2009-09-01 09:58 PM
0 Kudos
Reply

7,954 Views
MedicalApplicat
Contributor III

A:    The customer benefits of the Medical USB stack are as follows:

·           Complimentary

·           Standardization

·           Connectivity

·           Portability

0 Kudos
Reply

7,954 Views
MedicalApplicat
Contributor III

A:The stack contains HID, PHDC, CDC and MSD. Personal Health Care Device Class (PHDC) is the key component that allows USB connectivity for dedicated medical applications.

0 Kudos
Reply

7,954 Views
MedicalApplicat
Contributor III

A: General technical support on how to use the stack “as is” will be provided through our regular support channels (www.freescale.com/support). Support for customizing the stack is also provided. Due to the open nature of the stack, no support is provided for modification on existing classes or low level drivers of this stack.

0 Kudos
Reply

7,954 Views
MedicalApplicat
Contributor III

A:  Yes. The software is distributed freely and customers can add up classes while using within Freescale portfolio..

0 Kudos
Reply

7,954 Views
MedicalApplicat
Contributor III

A: The medical USB stack is complimentary while using within Freescale portfolio.

0 Kudos
Reply

7,954 Views
MedicalApplicat
Contributor III

A:    IEEE 11073 provides structure to your communication interface.

•          Defines commands to access data

•          Structures data to be transmitted

•          Defines communication states

0 Kudos
Reply

7,954 Views
MedicalApplicat
Contributor III

A:    USB.org Personal Health Care Device Class is a standard Implementation of USB communication for medical devices in the industry.

0 Kudos
Reply

7,954 Views
MedicalApplicat
Contributor III

A:    The Continua Alliance is a forum of member companies (+200) that have come together to form workgroups to set standards for medical systems.

0 Kudos
Reply