Maximum Bus frequency.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Maximum Bus frequency.

ソリューションへジャンプ
1,671件の閲覧回数
akashpandey
Contributor II

Hi,

I am using 8 bit freescale microcontroller MC9S08AW16A.i want to know following information-

1.Maximum bus frequency i can generate using an external oscillator in above controller.

2. If i use maximum Bus frequency then if there is any change in controller's perfomance?

ラベル(1)
タグ(1)
1 解決策
1,579件の閲覧回数
Encoder1
Contributor III

Hi Akash,

I am using 9S08AC16a and 9S08AC60 which are nearly identical to -AW family in different designs with internal oscillator and BusClock from 1 to 20MHz with no problems. External crystals are specified to work from 1 to 16 MHz (8MHz BusClock) but externally provided clock may be as high as 40MHz, i.e. full speed.

I had no problems to progressively increase BusClock from lower frequency ut to maximum other than on tasks which were based on (low) clock speed for delays. All minor problems, easy to fix. Performance always increased as well as you may expect with speed.

Salvatore

元の投稿で解決策を見る

1 返信
1,579件の閲覧回数
Encoder1
Contributor III

Hi Akash,

I am using 9S08AC16a and 9S08AC60 which are nearly identical to -AW family in different designs with internal oscillator and BusClock from 1 to 20MHz with no problems. External crystals are specified to work from 1 to 16 MHz (8MHz BusClock) but externally provided clock may be as high as 40MHz, i.e. full speed.

I had no problems to progressively increase BusClock from lower frequency ut to maximum other than on tasks which were based on (low) clock speed for delays. All minor problems, easy to fix. Performance always increased as well as you may expect with speed.

Salvatore