Maximum Bus frequency.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Maximum Bus frequency.

跳至解决方案
1,576 次查看
akashpandey
Contributor II

Hi,

I am using 8 bit freescale microcontroller MC9S08AW16A.i want to know following information-

1.Maximum bus frequency i can generate using an external oscillator in above controller.

2. If i use maximum Bus frequency then if there is any change in controller's perfomance?

标签 (1)
标记 (1)
1 解答
1,484 次查看
Encoder1
Contributor III

Hi Akash,

I am using 9S08AC16a and 9S08AC60 which are nearly identical to -AW family in different designs with internal oscillator and BusClock from 1 to 20MHz with no problems. External crystals are specified to work from 1 to 16 MHz (8MHz BusClock) but externally provided clock may be as high as 40MHz, i.e. full speed.

I had no problems to progressively increase BusClock from lower frequency ut to maximum other than on tasks which were based on (low) clock speed for delays. All minor problems, easy to fix. Performance always increased as well as you may expect with speed.

Salvatore

在原帖中查看解决方案

1 回复
1,485 次查看
Encoder1
Contributor III

Hi Akash,

I am using 9S08AC16a and 9S08AC60 which are nearly identical to -AW family in different designs with internal oscillator and BusClock from 1 to 20MHz with no problems. External crystals are specified to work from 1 to 16 MHz (8MHz BusClock) but externally provided clock may be as high as 40MHz, i.e. full speed.

I had no problems to progressively increase BusClock from lower frequency ut to maximum other than on tasks which were based on (low) clock speed for delays. All minor problems, easy to fix. Performance always increased as well as you may expect with speed.

Salvatore