MS08 DZ60 SCI Signal-Wire Operation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MS08 DZ60 SCI Signal-Wire Operation

1,663 Views
qiongyu
Contributor I

Hi,

When i use the Signal-Wire mode of the SCI on the chip of MS08DZ60, I met a problem. When i send some bytes vai the TXD pin, the SCI will occur trannsmit complete interrupt, but the receive buffer full interrupt is not occurs. In the datasheet, it says when In single-wire mode, the internal loop back connection from the transmitter to the receiver causes the receiver to receive characters that are sent out by the transmitter. So the transmitter is connect to the receiver, why no receive interrupt occurs?

Labels (1)
0 Kudos
Reply
0 Replies