MS08 DZ60 SCI Signal-Wire Operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MS08 DZ60 SCI Signal-Wire Operation

1,683件の閲覧回数
qiongyu
Contributor I

Hi,

When i use the Signal-Wire mode of the SCI on the chip of MS08DZ60, I met a problem. When i send some bytes vai the TXD pin, the SCI will occur trannsmit complete interrupt, but the receive buffer full interrupt is not occurs. In the datasheet, it says when In single-wire mode, the internal loop back connection from the transmitter to the receiver causes the receiver to receive characters that are sent out by the transmitter. So the transmitter is connect to the receiver, why no receive interrupt occurs?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)