MPXY 8600

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPXY 8600

2,283 Views
riccardocescato
Contributor I

Hi,

I need a clarification about the functional modes of the MPXY8600 sensor.

The datasheet says:

 

-"The Stop2 mode found in other Freescale S08 family members is not available; but the Stop3 mode is also present like other members of

the Freescale S08 family members." -

 

But there is no specification about how to set it.

In the SPMSC2 register I can write only the PDC bit while the PPDC, that was present in the mpxy8300 family, is reserved.

 

So, how can I set the Stop 3 Mode?

 

Can I equally write this last bit of the SPMSC2 register to obtain a Stop 3 Mode?

 

Thanks,

Riccardo

Labels (1)
0 Kudos
Reply
3 Replies

1,985 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Riccardo,

here is stop3 sample code i ever made for HCS08 JM60.  you could refer it to your project,

===============================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 Kudos
Reply

1,985 Views
riccardocescato
Contributor I

Hi Zhang,

I read your project but I can't understand where you set the Stop Mode.

In the main.c you set only the KBI and the Timer.

I can't see any setting for the register SPMSC2 so I can't understand how it is possible that the JM60 can go in Stop 3 Mode.

Can you explain me briefly?

Thanks,

Riccardo

0 Kudos
Reply

1,985 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Riccardo,

SPMSC2: PPDC bit is to control whether stop2 or stop3 selected.

0 Stop3 mode enabled.

1 Stop2, partial power down, mode enabled.

the default value of PPDC is 0, so the default stop mode is stop3. that's the reason I didn't set SPMSC2: PPDC in  sample code.

when execute   __asm STOP  , program goes into stop3 mode.

The code have two interrupt: timer and KBI

- when code is running, it is in stop3 mode, timer can not work

- when KBI happens(KBI #0), it wake up stop3

- go on running code, timer can work now.

===============================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 Kudos
Reply