MMA7260Q - sleep mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA7260Q - sleep mode

2,846 Views
UcTechnoGeek
Fresh Out Contributor
Sorry for asking a non-mcu question here, but does anyone know if the MMA7260Q accelerometer has a built in pull-up on the /sleepmode pin?
 
I know I can just pull it up, but do I have to?
 
uCTechnoGeek
Labels (1)
0 Kudos
Reply
3 Replies

1,645 Views
bigmac
Specialist III
Hello,
 
According to the data sheet, there are apparently built-in pull-down resistors on the g-select inputs, but nothing internally on the sleep mode pin.
 
Note that the active state of this pin is hign, so the use of an external pull-down resistor (rather than pull-up) would give lower current in sleep mode.
 
Regards,
Mac
 
0 Kudos
Reply

1,645 Views
Mayu
Contributor I

My question is about MMA7260q hardware too, I was reading its datasheet  and I have connected mma6270q as indicated by the datasheet  but I can't get the right values when x es (+1g) ->2.45v or close to it I only got 1.8-1.9v and when x(-1g) I got 1.4v and is the same in y and z axis  why?

 

I hope  you can help me

 

 

 

0 Kudos
Reply

1,645 Views
bigmac
Specialist III

Hello,

 

To achieve a +1g voltage of 2.45 volt would require that the device be set to the highest sensitivity of 800 mV/g.  It appears that you may currently have the lowest sensitivity setting of 200 mV/g.  The nominal output would be 1.85 volt for +1g, and 1.45 volt for -1g, with this setting.

 

Regards,

Mac

 

0 Kudos
Reply