Hi,
I'm programming a MM908E626 controller with;
- M68HC08EY16 microcontroller
- a H-bridge with current limiter settings, controlled via SPI.
I have set the Current Limiter Setting (CLS) at different values.
I have tried different values PWM signals on FGEN.
I have used different FGEN values but all within the specified recommended settings.
PROBLEM:
unfortunatly the output of the h-bridge is not re-enabled on every rising FGEN! Therefore the current isn't smoot , not even with a 20Khz pwm on FGEN !!
Why isn't the output re-enabled ?
how I did applied the specifications in read the datasheet:
The datasheet of the MM908E626 specifies the H-bridge. On page 27 of the datasheet a picture(figure 13. Half-bridge current limitations) explains that:
1. The half-bridge output is disabled when the set current limit is reached.
2. When the current limit did disable the half bridge, a rising edge on the FGEN input would re-enable the output again.
With this information in my mind I programmed a PWM signal from the microcontroller to the FGEN input of 20 Khz, 50uS interval. I did use a scope to verifie that this signal was now present on the FGEN input !! I did use the scope-input 1 to check on different FGEN values and I did use input 2 to measure the h-bridge output. I used the FGEN to trigger the signal.

Channel B = FGEN signal
Channel A = Current out of h-Bridge to Brushed Motor
Set current limit was 740mA