MCU in MC13213

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU in MC13213

1,734 Views
Thomas_H
Contributor I
Hello,

please could anyone tell me which controller is in the MC13213 RF transceiver? It should be an MC9S08GB60 or a MC9SGT60.

regards
Thomas
Labels (1)
0 Kudos
Reply
1 Reply

1,117 Views
peg
Senior Contributor IV
Hello and welcome to the forums Thomas,

The chip inside a GB60 and a GT60 is exactly the same.
The are all mask xL31R (x = 1 to 4)
The GT simply has less pads bonded out to pins.
The MC13213 does not have all pins bonded out either and so is closer to a GT.
You can still use the higher timer channels and such, you just don't have the channel pins etc.

With the A versions of the GT they have actually cut down the die to more closely tie in with what is actually bonded out.
But I believe the Zigbee stuff still uses the old GB/GT (non-A)

0 Kudos
Reply