Hi Mac,
shame the jig wouldnt allow export of the S record. In the manual for the JICS kit it specifically says in the troubleshooting section, that if the C8A needs replacement, programmed devices are available from Motorola, or you can download the S record from the BBS and do it yourself. It also says the file is available on www.design-net.com/ etc etc but I see that URL is now parked.
I'll have a play with the Kit and see if it is tucked away anywhere - it's not on the CD that came with the kit.
Nevermind....... didnt think it would be so easy ! 13 years in embedded is a lifetime :smileyhappy:
Thanks,
Chris