MCF51QE32 BDM Multiling connection failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCF51QE32 BDM Multiling connection failure

1,823 Views
fidellyo
Contributor I

Hi there,

 

I am new to the 32 bits ColdFire MCU and I had some experience with 8 bits MCU...

I have a demo board qg8 that has a multilink BDM that can be used to flash an 8 bits MCU (external MCU like HCS08QE8 and others, I managed to connect to these external devices with success based on this thread: http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&message.id=12921...) .

 

I want to connect to the ColdFire V1 MCU ( I made my own board) but unfortunatelly without any success!!!!! 

 

I am using CodeWarrior 6.2 with Patch 6.2.2 and PE 3.04 (the latest one). When I attempt to connect the ColdFire it gave me a failure error (Failure connecting the the device, Power cycle the ColdFire V1 processor....) but it autodetect the ColdFire device!!!.

 

any one had a success to connect this device? 

any help is appreciated!.

P.S: I search this forum for any thing that help me but without success.

 

Thanks to all...

Labels (1)
0 Kudos
Reply
3 Replies

869 Views
fidellyo
Contributor I

No one have experience with ColdFire V1!!!! Please if any, just give me any suggestion.

 

Thanks.... 

0 Kudos
Reply

869 Views
bigmac
Specialist III

Hello,

 

It might have helped your situation if this query had been posted to the Coldfire forum, rather than the 8-bit forum.

 

Regards,

Mac

 

0 Kudos
Reply

869 Views
fidellyo
Contributor I

Hi Bigmac,Thanks for your reply... I put this on the CF forum and I hope that someone can give me any suggestion.... I thought that it is better to put this query into the 8 bits forum because ColdFire V1 uses the same BDM and CodeWarrior as the 8 bits MCU!!!!!. 

0 Kudos
Reply