MC9SGB60: writing to KBISC during keyboard interrupt ignored

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9SGB60: writing to KBISC during keyboard interrupt ignored

744 次查看
petervittali
Contributor I

This is the code:

 

#define Vkeyboard 22
#define ON 0
#define OFF 1
#define LED1 PTFD_PTFD0
#define LED2 PTFD_PTFD1

 

interrupt Vkeyboard void intCLK() {
 
  LED1 = !LED1;
  KBI1SC &=  0x0f;  // (1) commenting out this will render ineffective statement (2)
  KBI1SC_KBACK = 1;   // clear interrupt
  KBI1SC_KBEDG4 = 1;  //  (2) wait for rising edge
}

 

void main(void) {

 

  /* LEDs are output*/
  PTFDD = 0x03;
  LED1 = OFF;
  LED2 = OFF;
 
  KBI1SC = 0x02; // request HW , edge only
  KBI1SC_KBEDG4 = 0;  // first wait for falling edge
  KBI1PE_KBIPE4 = 1;
  EnableInterrupts;

 


  for(;;) {
    __RESET_WATCHDOG();
  }
  /* please make sure that you never leave main */
}

 

During the keyboard interrupt handler, I want to change the edge behavior ( from falling to rising ). This works as long as I

outcomment line (1) where I write to KBI1SC register. If do this write, the command KBI1SC_KBEDG4 is ignored, that is the edge dectection remains falling edge. Worse, after a couple of changes , the keyboard interrupt stops working all toegether.

 

I use the Axion demoboard for the GB60 with an external debounced push button.

 

What's wrong with that write to KBI1SC inside the interrupt handler ?

 

Thanks for your support

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数