MC9S08RE16 stop3 current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08RE16 stop3 current

2,916件の閲覧回数
stevec
Contributor III
I have an  MC9S08RE16 set into stop3 mode and get a current of 1.2mA (down from 4.9mA running with 16MHz crystal). This is a rather more than I expected. Can someone give me some pointers as to how to reduce this. 

Steve
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,384件の閲覧回数
tonyp
Senior Contributor II
If you have any floating pins, tie them or pull them to either Vdd or Vss.

Is this pure STOP3 you're measuring?  Or, do you periodically wake up to service some interrupt, possibly more often than you had expected?
0 件の賞賛
返信

1,384件の閲覧回数
stevec
Contributor III
I'm planning on pure stop3. Nothing to wake it up except the KBI function. I have put together a circuit with only the uP on it, all peripheral chips have been omitted. I have made all pins as o/ps before going into stop3 mode and this then gives me 0.9mA instead of 1.15mA stop3 current. 0.9mA if o/ps are set high or low.
0 件の賞賛
返信

1,384件の閲覧回数
Nik
Contributor III
Hi Steve,
You are having better luck than I am.  When I enter STOP3, the XOSC continues to run. 
I tried STOP2, the crystal stops, but it won't wake up.  Well, the crstal does, but that's it.  This is a MC9S08JM60.
 
Regards,
-
Robert
0 件の賞賛
返信