MC9S08RE16- need two timers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08RE16- need two timers

2,420 Views
stevec
Contributor III
I am running a 1mS timer under interrupt as a system clock. I need to independantly determine a fixed 62.5uS timer to achieve a 16kHz speech output sample rate i.e start 62.5uS timer, output to DAC, wait for timer to time out. How can I achieve this with only the one timer module (if at all).
Labels (1)
0 Kudos
Reply
3 Replies

1,294 Views
bigmac
Specialist III
Hello,
 
It is not clear how you have already configured the timer for your 1ms tick.  However, there would appear to be a couple of alternatives, using either one or two channels of the TPM module, in output compare mode.  In both cases, the TPM modulo setting should remain at its default, with a free-running counter.
 
The first alternative would be to use separate channels for each of the intervals.  When an interrupt occurs following each output compare event, simply add the number of increments corresponding to the required interval to the current channel value.
 
The second possibility would require only a single TPM channel, again using output compare mode (normally interrupt only configuration), to generate an interrupt every 62.5 microseconds.  Then within the ISR, increment a count value.  One in every 16 interrupts would then correspond with the `1ms tick.
 
count++;      // Every 62.5us
if (!(count & 0x0F))
   tick = 1;  // Every 1ms
 
Regards,
Mac
 


Message Edited by bigmac on 2008-09-10 01:34 PM
0 Kudos
Reply

1,294 Views
stevec
Contributor III
Thanks Bigmac,

So I can not run two independant timers. I see that now as there is only one counter. I was trying to reduce interrupt processing time as my speech output routine takes 47 uS. I don't have much time left within the 62.5 uS sample period to do other things like switch debounce. I may have to review whether I go back to the AT89F51 I was using before (which has 2 timers). When I chose this particular HCS08 chip I was mislead by the manual into thinking that the CPU executed instructions at a higher rate (xtal freq rather than xtal freq/2) so I though I had lots of clock cycles to get things done in.
I will look at your suggestions however and see which has the lowest overhead.
0 Kudos
Reply

1,294 Views
bigmac
Specialist III
Hello,
 
To avoid the additional complexity (and execution cycles) of handling nested interrupts, it sounds like the 1ms tick should be derived within the 62.5 us interrupt routine.  This way you will avoid the potential for the additional overhead of a second interrupt to delay the priority interrupt.
 
I assume you would be using the maximum bus frequency of 8MHz, with 500 bus cycles between successive interrupts.  You may need to use inline assembly code for the ISR to minimize the number cycles required.
 
In pure assembly code, the minimum overhead to enter the interrupt, update the OC value, clear the interrupt flag, and exit the interrupt would amount to about 40 cycles (5 us).  Here, I assume a prescale value of 4 for the TPM.  To further set a 1ms tick flag, for eventual processing as a background task, would need an additional 13 - 17 cycles within the ISR.  With this optimised code, the total overhead should amount to about 7.1 us.  Obviously, this would not leave many cycles for background processing tasks.
 
For the purpose of the calculation, here is the assembly code that I assumed -
 
ISR_TPMCH0:             ; [11] Entry to ISR
     pshh               ; [2]
     ldhx  TPMC0V       ; [4] Update TPM channel
     aix   #125         ; [2]
     sthx  TPMC0V       ; [4]
     inc   COUNT        ; [5] Global variable in zero page
     lda   COUNT        ; [3]
     and   #$0F         ; [2] Mask low nybble
     bne   BR1          ; [3] Branch if not timeout
     mov   #1,TICK      ; [4] Global variable in zero page
BR1:
 
     ; Other code here
 
     bclr  CH0F,TPMC0SC ; [5] Clear flag
     pulh               ; [3]
     rti                ; [9]
 
Could there be a possibility that your speech output routine would benefit from the use of assembly code (if you are not already doing so)?
 
Regards,
Mac
 
0 Kudos
Reply