MC9S08PL4 schematics review

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08PL4 schematics review

Jump to solution
3,751 Views
shai_b
Senior Contributor II

Hello Team,

My Customer has a plan to use MC9S08PL4 and they want to review their schematics and get your recommendations for the mass-production stage, can I open a private ticket to be able to share the full schematics?

besides that, below you can find part of the drawing 

mc9s08pl.png

Can you please confirm that Pin 1,2,3,4 are for flashing the firmware? thanks in advance

Regards,

Shai

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,590 Views
vicentegomez
NXP TechSupport
NXP TechSupport

I will answer on the ticket

Have a good day

View solution in original post

0 Kudos
Reply
5 Replies
3,590 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

yes, in order to program the device you need the PTA4 (BKGD), PTA5 (Reset) VDD and VSS.

So yes the pins are ok.

If you want you can send me the schematic directly to me

In some time and depending the application maybe you will need to add an external pull up on the BKGD pin.

Regards

Vicente Gomez

0 Kudos
Reply
3,590 Views
shai_b
Senior Contributor II

Dear Vicente Gomez,

Please find attached, customer schematics for review (you find below his requirements)

BTW, I have suggested him to add a capacitor of 0.1uF on the RESET pin and VSS(GND)

Second thing, there is any way to flash the device using the UART(RX/TX) pins?

Please advise back how I can share with you the schematics, thanks in advance

BTW, you can feel free to send me a mail at [email protected] 

Best Regards.

Shai Berman, 

0 Kudos
Reply
3,590 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

I have already created a new ticket for this case, you can send me all the information on this ticket

regards

Vicente 

0 Kudos
Reply
3,590 Views
shai_b
Senior Contributor II

Hi Vicente,

Thanks, I have uploaded the schematics for reviewing, a fast response will be highly appreciated.

Best Regards.

Shai Berman

0 Kudos
Reply
3,591 Views
vicentegomez
NXP TechSupport
NXP TechSupport

I will answer on the ticket

Have a good day

0 Kudos
Reply