MC9S08MP16 problem with upload program on it using BDM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S08MP16 problem with upload program on it using BDM

1,981 次查看
pawelniewiadoms
Contributor I

Hello, I have MC9S08MP board and I have problem to upload program on it via BDM. I'm using CodeWarrior 10.6 and when I'm trying debug example program this window appears:118699_118699.pngpastedImage_0.png

When I reconnect it nothing happens. After click OK this appears:

118700_118700.pngpastedImage_1.png

Then it's just error when I click 'Abort'. OSBDM is visible in device manager and all drivers are installed properly.
Please help me with this problem.
Greetings,
Pawel Niewiadomski

标签 (1)
0 项奖励
回复
2 回复数

1,891 次查看
pawelniewiadoms
Contributor I

Problem solved, It was problem with one of resistors in my board which has short circuit. Thanks for responding!

0 项奖励
回复

1,891 次查看
Leojunin
Contributor IV

Hi Pawel,

check the bypass capacitor, there may be a lot of capacity in the power line and prevents micro finalize the POR. It would be nice some 100nF I have not tried more, but if I had that fails. You can skip this failure by setting the Power Down Delay longer. Example: 1S

Best regards

0 项奖励
回复