MC9S08LG32 LCD Module Voltage?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S08LG32 LCD Module Voltage?

1,532 次查看
sandeepnaik
Contributor I

I am using MC9S08LG32 (LQFP-80 package) with inbuilt LCD Module.

I am operating my core and other peripherals at 3.3 VDC.

Can I still operate my LCD Module from 5 VDC power-rail without damaging the controller.

标签 (1)
0 项奖励
回复
1 回复

1,355 次查看
philip_drake
NXP Employee
NXP Employee

Hello sandeepnaik,

The LG32 has an integrated LCD driver that can supply LCD waveforms for 5 V glass.  You can use the on-chip charge pump to create the 5V source needed to drive the LCD when operating the MCU at 3.3V.

The only time you should connect VLL3 to 5 V is when the MCU voltage is set at 5 V. 

The externally supplied voltages MUST NOT EXCEED VDD :smileysad:.

Check out the reference manual, LCD section 

Table 9-19. LCD Power Supply Options.

http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MC9S08LG32RM.pdf?fpsp=1

Regards,

Philip :smileyhappy:

0 项奖励
回复