MC9S08LC60: Why is stop mode being reset?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08LC60: Why is stop mode being reset?

1,394 Views
MotownSide
Contributor I

Hi,

 

We are unable to get into any stop mode. The current is always high ~4mA. It seems that when we enter stop mode, it is immediately being reset. We are interested in getting into stop3 mode.

 

We followed the settings in the datasheet. (Table 3.1)

Below is the settings we set for stop3 mode

 

  SOPT1_STOPE=1;

  SPMSC1_LVDSE=0;

  SPMSC1_LVDE=0;

  SPMSC2_PDC=1;

 

Is there something else that we overlooked?          

Labels (1)
0 Kudos
Reply
1 Reply

977 Views
bigmac
Specialist III

Hello, and welcome to the forum.

 

Have you allowed that the SOPT1 register is "write once"?  This means that all bits of the register, including the STOPE bit, must be simultaneously written, usually early in the initialisation process.  It is not possibly to set bits individually, and if this is what you are attempting, it may mean that the STOP instruction is never enabled, resulting in an illegal opcode reset when you attempt to enter stop mode.

 

Regards,

Mac

 

0 Kudos
Reply