MC9S08JM60 USB-CDC device problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S08JM60 USB-CDC device problem

2,785 次查看
stéphanec
Contributor I

Hello everybody,

 

I used the last USB-STACK proposed by freescale (the 4.0.3) with a MC9S08JM60 to develop a USB-CDC application.

 

With my DEMOJM development card, I have used the example provided in the Stack ("C: \ Freescale \ Freescale USB Stack v4.0.3 \ Source \ Device \ app \ cdc \ CW10 \ s08usbjm60"). I also used tools from the excelent blog "mcuoneclipse.com" (USB or not: CDC with Processor Expert | MCU on Eclipse). I have obtained two USB-CDC devices. Well !

 

When I connect my USB-CDC devices directly into an USB port on my PC, there is no problem, the devices are both detected and the driver (CDC.inf) works. I can connect and communicate with my JM60 demo board across the CDC protocol.

 

My problem is when I connect the USB-CDC devices to my USB over IP module (StarTech - Part # USB1000IP). The USB devices are detected and appear inside the Windows Device Manager, but not installed inside the ports (COM and LTP) section. And the device is not available for communication. I tried two other USB over IP modules from other manufacturers, and I have the same problems. Worse, if I try to force the driver installation, Windows 7-64 or XP-32 show me the blue screen.

 

For info : inside the Windows Device Manager, the device instance id is : "USB\VID_2504&PID_0300&REV_0002" when I connect the device directly to USB.

It becomes "USB\Vid_2504&Pid_0300&Rev_0002&MI_00" when I use the  USB over IP module


Do you have a solution? An idea? A line of thought

 

Thank you in advance for your help.

 

Best Regards

 

Stéphane

 



标签 (1)
标记 (4)
0 项奖励
回复
2 回复数

1,791 次查看
DerekLau
Contributor IV

Try by modifying the inf file to add one more line as below

XXXXXXXXX (the string that you use in the inf file), USB\VID_2504&PID_0300&MI_00

0 项奖励
回复

1,791 次查看
stéphanec
Contributor I

Hello,

Thank you for your answer.

I've thought about this solution. Unfortunately it does not work (crash the PC at driver installation).

Best regards,

Stéphane


0 项奖励
回复