MC9S08JM16 based device - USB troubleshooting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08JM16 based device - USB troubleshooting

853 Views
dekkard
Contributor I

Hello,

I apologize if this is not the correct forum to post this kind of questions on. Please, let me know if there's a more suitable one.

To the topic - I've got a device built upon a MC9S08JM16 (a USB keyboard), which has a connectivity problem. When the keyboard is plugged into a computer USB port, it's not detected by an OS, and there's completely no USB interaction going on as can be seen by a USB analyzer program.

The microcontroller itself gets power and looks operational - I could dump its firmware and verfy it via USBDM. Also, it appears to be scanning the key matrix of the keyboard, as it should. The only problem is that the voltage on V usb33 is much less than 3.3v and there's almost no voltage on the USBDP (D+) and USBDN (D-) pins.

Is there any possibility this problem can be diagnosed and fixed?

If so, where do I start from and what should I check first?

0 Kudos
Reply
1 Reply

836 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Are you using a custom board?

 

Are you using any sample code?

Is there any hardware problem?

Missing parts? 

 

0 Kudos
Reply